Hi all,
I'm using DM814x EVM with video conference application board (EZSDK version 05.03.01.15).
I would like to know if it is possible to capture audio using the HDMI input.
Thank you,
Simon
do u have hdmi receiver on DM8148 EVM?
Manoj
Yes, on the daughter card (video conference application board rev B)
Hi,
HDMI receiver on VC daughter cards supports audio. But we dont have driver for that.
Regards,
Hardik Shah
Please mark this post as answered via the Verify Answer button below if you think it answers your question. Thanks!
Hi Hardik,
Thanks for the answer,
Are you planning to support it in a futur EZSDK release?
Hi
Sorry for interrupt.
I am almost doing the same thing described in this post.
I am also curious about HDMI audio capture driver
However, I have a custom board with a ITE HDMI receiver.
Jun
We dont have plan to support HDMI Audio input on SIL9135 as of now.
Regards.
Hi Hardik
Do you have any suggestions if we are going to develop our own hdmi audio capture driver?
Where should be start from?
Jun,
How did you end up handling your HDMI input issue?
Thansk.
Mike.