Hi,
I would recommend waiting for the latest EZSDK release. The HDVPSS binaries that present in the PSP package contain only the driver interfaces and not the full multimedia stack. Hence they have not been verified with OMX, GStreamer etc.
--Sid
Need more information? Some Categories on TI's processors wiki are -
http://processors.wiki.ti.com/index.php/Category:DaVinci
http://processors.wiki.ti.com/index.php/Category:DaVinci_Linux
http://processors.wiki.ti.com/index.php/Category:EZSDK
http://processors.wiki.ti.com/index.php/Category:DVSDK
http://processors.wiki.ti.com/index.php/Category:OMX
Hello Siddharth Heroor:
Thanks for your reply, I will wait for the latest EZSDK,Thanks.
Wheather Video Frame Processing Componnet/Video Decode Component On Dm81XX support the 25fps Video file?May be it can't.
Now,I want to play the 25fps H264 HD(or SD) video file with gstomx(or OMX or gstreamer ),but I foud the result is not very good. If I convert the 25fps video to 30fps,then can play well,So,What can I do if I want to play the 25 fps H264 video? I only have the dm814x_hdvpss.xem3 and dm814x_hdvicp.xem3 bin files,So where I can download the source code if I want to change the H264 decoder algorithm.
Thanks very much.
Regards .zhichao.