Hi ALL,
We want to get 720p on DM8127IPNC,we have got the raw image with DCC,but got nothing when saving yuv image with DCC(The streaming is active,but nothing from UI),seems the IPIPE didn't work.
So any idea to check which part of IPIPE didn't work?
Best Regards,
Xiang,
Are you using the IPNC RDK software release?
If so, with 720 - do you see the streaming working? The YUV is IPIPE->RSZ output which is the same buffer which goes to encoder for the streaming usecase.
Regards
Rajat
--------------------------------------------------------------------------------------------------------------Please click the Verify Answer button on this post if it answers the question.--------------------------------------------------------------------------------------------------------------
Hi Rajat,
Thanks for your reply,I am using the IPNC RDK V2.0.
Yes,it's very strange,i can see the live streaming,but the streaming in UI just keep blinking,seems hanged at the first frame.
By the way,is there any plan in your future release which supports switching resolution dynamiclly?
Hi Xiang,
Dynamic resolution change will be supported in the upcomming release ver2.8.0. This is currently planned for next week.
Please sync with the local FAE at your end to get the release.