Hi all. I use a qemu-debuootstrap to build a ubuntu 12.10 rootfs for a dm8148 board .And using the ti firmware file and configs from the RDK,with a kernel 2.6.37.
The kernel and rootfs is boot ok and all firmware was load correctly.
But as I apt-get insatll the lxde ,and xorg, I can't the the x run.
startlxde tellme ther's no display, and cmd X get error and exit.
X -configure error with "no devices to configure".
I think the xserver didn't connect with the graphic dirvers for now.
Can somebody give me some hint on this?