Hi All,
- We are going to start new project based on DM8148 and AM3505.
- In this project we want to use internal switch of DM8148.
- In this case, the AM3505 will be connected directly via RMII interface to EMAC1 port of DM8148.
- which should be configured to static 100Mb full duplex configuration
- The direct implication is that the DM8148 must be turned on and enable the switch in order that AM3505 will have external Ethernet connection through the RJ-45 port.
- In order to implement the above, DM8148 u-boot must enable the internal Ethernet switch.
- Current official u-boot from TI supports only single EMAC0 port and the switch is enabled only from Kernel space.
- For reference I have attached image "ethernect_connection.".
- First of all I want to know that is it feasible to connect DM8148 ethernet switch with given connection shown in image?
- If it is feasible then can we configure DM8148 3PSW switch from u-boot to enable EMCA0 and EMAC1 port?
Regards,
Jemish