Hi All,
We are using IPNC_RDK 3.5 for DM8127 processor.
We are trying a use-case as given below.
USECASE-1 :
In this usecase, We are facing problem with YUV frames at A8. YUV frames of YUV CH1 comes with an OSD of STREAM CH0 and STREAM CH1, and YUV frames of YUV CH0 comes with an OSD of STREAM CH0.
So, here both YUV Channels comes with an OSD without applying on it, YUV CH1 with two OSD and YUV CH0 with single OSD.
I have attached the snapshots for both YUV channels.
If we use-case(use-case 2) as given below, then everything is working fine. Both YUV channels don't have any OSD on them.
In this use-case we have connected DUP 1 next to the DEI link and FD link next to the SCALAR link.
USECASE - 2:
In both use-case, we are using DEI as a scalar.
We don't understand why this is happening?. Kindly help us to resolve the problem.
Your answers will be helpful to us.