Hi,
We are working on DM8127 platform and using IPNC RDK 3.5
H.264 codec version : 02.00.04.01
H264 encoder create time parameter settings are:
maxBitRate = -1;
encodingPreset = 3
rateControlPreset = IVIDEO_USER_DEFINED;
enableHighSpeed = 0;
format = 9
profile = 100
dataLayout = 0
fieldMergeEncodeEnable = 0
enableAnalyticinfo = 0
qpMin = 10
qpMax = 40
qpInit = -1
Folowing parameter dynmically set for VBR mode
rateControl = ALG_VID_ENC_RATE_CONTROL_VBR (0)
targetBitRate = <inputBitRate>
reteControl is set with ENC_LINK_CMD_SET_CODEC_RATECONTROL control command and targetBitRate is set with ENC_LINK_CMD_SET_CODEC_BITRATE control command.
How Bitrate will vary with complex scenario means up to what limit targetBitrate value goes for complex scenario ?
For example, If we set targetBitRate as 8Mbps (1080p resolution) then what would be maximum bitrate value for complex scenario ?
Thanks,
Rachit