Hello everyone!
I'm using IPNC RDK ver3.5 for 8127 and I met a problem in dealing with memory.
I need to load a data file(named "model.bin") into the memory,for my dsp alg will use
these datas.
Firstly,I've tried function fread to read these datas in my alg,but it seems not work.
Then,I use the command "tftp 0x8fb00000 model.bin" to load the data into SDRAM ,the
address is calculated ahead of time which locates in DSP data.I think I can access this
memory directly using pointer or whatever,but this time I can't get data either.It really
confuses me.
Has anyone done the similar thing ? I need some advice!
regards
yu