Dear All,
I am working with a custom board using DM8127 dsp. It's based on IPNC RDK v3.5. In system_dctrl.c, we use VPS_DC_CIG_CONSTRAINED_OUTPUT as the input node of VPS_DC_DVO2_BLEND. But we got the constrained output data since the digital value of Y is clipped to [16-235]. If we want to get the full range data of YPbPr from DVO2, how can we set in system_dctrl.c ?
Below is my settings:
links_m3vpss\system\system_dctrl.c:
Vps_DcConfig gSystem_dctrlTriDisplayConfig = {
VPS_DC_USERSETTINGS, /* Use Case */
/* Edge information */
{
{VPS_DC_BP0_INPUT_PATH, VPS_DC_VCOMP_MUX} ,
{VPS_DC_VCOMP_MUX, VPS_DC_VCOMP},
{VPS_DC_CIG_NON_CONSTRAINED_OUTPUT, VPS_DC_HDMI_BLEND},
{VPS_DC_CIG_CONSTRAINED_OUTPUT, VPS_DC_DVO2_BLEND} ,
{VPS_DC_SEC1_INPUT_PATH, VPS_DC_SDVENC_MUX} ,
{VPS_DC_SDVENC_MUX, VPS_DC_SDVENC_BLEND} ,
{VPS_DC_GRPX0_INPUT_PATH, VPS_DC_HDMI_BLEND} ,
{VPS_DC_GRPX0_INPUT_PATH, VPS_DC_DVO2_BLEND} ,
{VPS_DC_GRPX2_INPUT_PATH, VPS_DC_SDVENC_BLEND},
{VPS_DC_MAIN_INPUT_PATH, VPS_DC_VCOMP},
{VPS_DC_AUX_INPUT_PATH, VPS_DC_VCOMP_MUX},
{VPS_DC_BP1_INPUT_PATH, VPS_DC_SDVENC_MUX},
}
,
12,
/* VENC information */
{
/* Mode information */
{
{VPS_DC_VENC_HDMI, {FVID2_STD_1080P_60}
}
, /* 1080p30 is mode
* is overwritten
* later inside
* System_displayCtrlInit
*/
{VPS_DC_VENC_DVO2, {FVID2_STD_1080P_60}
}
, /* 1080p30 is mode
* is overwritten
* later inside
* System_displayCtrlInit
*/
{VPS_DC_VENC_SD, {FVID2_STD_NTSC}
}
}
,
(VPS_DC_VENC_HDMI | VPS_DC_VENC_DVO2), /* Tied VENC bit
* mask */
3u /* Number of VENCs
*/
}
};
I will be very grateful if you can give me some hint for solving this problem.