Hi
I'm facing an issue on USB host port of a ti8148-based custom board ,when boot kernel with usb storage deivce plug in, kernel can detect the usb storage device. But, if I boot kernel without plug the usb storage device, and after kernel boot completely, I plug in the usb storage, the kernel can't detect the device, and print the following messages
musb_stage0_irq <== Power=f0, DevCtl=98, int_usb=0x80
musb->xceiv->state = 0x7
VBUS_ERROR in a_wait_vrise (99, VALID), retry #1, port1 00000100
and after these operation, any other usb devices can't be detected ether.
But when kernel boot completely, I plug in the usb mouse, the kernel can detect the usb mouse.
what's the problem about this issue?
Thanks