hi,
There are some questions about DCC, as follow:
(1) I get the information as that there is no header and foot in the data of YUV format save from DCC and the data is saved as YUV420SP(YYYY…UVUV…). However I can't show the right grayscale images when I get the first 1920*1080 data as Y from the *.yuv file.(PS: my picture is 1920*1080) I read the each data as uint8. I want to know whethet there are some wrong steps I take which lead me to get wrong image.
(2) the other question is about the exposure stepsize. I want to know the reason that we need to use 500,000 not other values in the following code.