hi,
platform: DM8127
sensor: ar0331 parallel (1080p 30 fpbs)
I want to integrate AR0331 sensor in DM8127 and source code of it is given in iss devices.
Is AR0331 source code tested with DM8127 camera or not?
Best Regards,
Prashant.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
platform: DM8127
sensor: ar0331 parallel (1080p 30 fpbs)
I want to integrate AR0331 sensor in DM8127 and source code of it is given in iss devices.
Is AR0331 source code tested with DM8127 camera or not?
Best Regards,
Prashant.
Prashant,
Are you using IPNC RDK?
Regards,
Pavel
HI Pavel,
Thanks for your reply.
Yes i am using IPNC RDK 3.8.
Best Regards,
Prashant.
Hi In IPNCRDK3.8 there is a file Rules.make,
In it , there is
ifeq ($(IPNC_DEVICE), DM8127)
IMGS_ID := IMGS_MICRON_MT9J003
#IMGS_ID := IMGS_MICRON_AR0330
#IMGS_ID := IMGS_MICRON_AR0331
#IMGS_ID := IMGS_PANASONIC_MN34041
#IMGS_ID := IMGS_OMNIVISION_OV10630
#IMGS_ID := IMGS_MICRON_MT9M034
else
which means AR0331 is already integrated and tuned .
Hi Wang,
Thanks for your reply.
Yes, AR0331 sensor source is given in IPNC RDK.
I just want to know that after flashing FPGA binary file to sensor board, can i directly run my demo on camera or is there any other changes needed?
Best Regards,
Prashant.
I guess so. Why not give a try ? Though I dont have AR0331 sensor board in hand.
FPGA just convert the serial port to parrallel, so I really dont think there is difference then other sensor board.
BR,
Eason
If you are using a sensor board from appro or leopard, just go ahead check w/ them.