Hi,
I am using IPNC RDK DM8127 reference kit, version 3.5, where try to implement 'tiler' module in full feature usecase.
Case 1:
IPNC_TILER_ENABLE := NO
BTE_ENABLE := NO
Rebuild by make -s all & Open WebUI.
There is an option in WebUI - Mirror (Horizontal & Vertical), & is worked on it.
Case 2:
I just did changes in Rules.make file & using full feature usecase.
IPNC_TILER_ENABLE := YES
BTE_ENABLE := YES
Then rebuild by giving a command => make -s all.
When I opened a WebUI, I got a green frame (actually no frame) on 1920x1080 resolution, where got a frame on 720x480 resolution. Why not getting frames on 1920x1080 ? Is there any memory issue ?
There is no option in WebUI like "90degreeRotate" or "270degreeRotate" ?
I observed, Mirror is worked in both cases..either IPNC_TILER_ENABLE is enabled or not enabled in Rules.make file. So, what is an effect of IPNC_TILER_ENABLE in Rules.make file ?
Waiting for your reply.
Thanks.
Sandip Gokani.