Hi,
I am using a DM8148 custom board in which the camera signals are connected to the CAM_D[0],CAM_D[1],...,CAM_D[7] lines in the processor.
Now I know that the OMX framework can be used for capturing video from VIN[0] or VIN[1] ports.
So, can we use the OMX framework for capturing video from CAM_D[0] interface?
If yes then can you please share some links for that or some documents if available?
Regards,
Debasish