Hello:
I am running the OMX decode_display sample(component-sources\omx_05_02_00_38\examples\ti\omx\demos\decode_display) with DM814X EVM board, but it's crash,
Does anyone have the same issue what cause the crash?
error log:
width: 1440
height: 1080
frame_rate: 60
gfx: fbdev disable
codec: h264
display_id: 0
Decoder-Display example
===============================
Syslink: _NotifyDrvUsr_eventWorker thread created, tid = 1224
Syslink: _NotifyDrvUsr_eventWorker: set real-time priority of 32
Osal runStub() thread, tid = 1227
Osal runStub(): set real-time priority of 32
OMX_Init completed
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
UIAClient is ready to send a UIA configuration command
UIAClient received UIA_CONFIGURE_ACK
UIAClient is done sending requests
opening file
Osal runStub() thread, tid = 1228
Osal runStub(): set real-time priority of 32
decoder compoenent is created
PADX: 32 PADY: 24
level set is 12
Osal runStub() thread, tid = 1229
Osal runStub(): set real-time priority of 32
Segmentation fault