Hello .
I am trying to dbg the linux kernel on DM8148 via JTAG XDS100V2 with no luck .
I am using the linux_lsp of the package DVRRDK_04.01.00.02 .
In order to change the .config file i changed the file 'DVRRDK_04.01.00.02\ti_tools\linux_lsp\kernel\linux-dvr-rdk\arch\arm\configs\ti8148_evm_defconfig'
because the build process override the .config file with that one .
In it i enabled manually :
CONFIG_DEBUG_INFO=y
CONFIG_ARM_UNWIND=y
CONFIG_FRAME_POINTER=y
After building the kernel the CONFIG_FRAME_POINTER disapears from the .config file .
when i load the target with the VMLINUX file i can not set breakpoints .
Am i missing something ?
Regsrds , Shlomo Kabaz .