Hi,
{0x00, 0x01},
{0x04, 0x57},
{0x0c, 0x12},{0x0d, 0x88},
{0x27, 0x58},
{0x17, 0x41},
{0x31, 0x02},
{0x3D, 0xA2},
{0x3E, 0x6A},
{0x3F, 0xA0},
{0x0E, 0x80},
{0x55, 0x81},
{0x0E, 0x00},
adv7180 register settings are set with above values.
firmware which is working on evmboard we are using on adv7180 , but It is not stopping properly after running gstreamer pluggin , captured file size is always zero
Run output:
root@dm814x-evm:~# gst-launch -e omx_camera ! filesink location=abc.yuv
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
Caught interrupt -- handling interrupt.
Interrupt: Stopping pipeline ...
EOS on shutdown enabled -- Forcing EOS on the pipeline
root@dm814x-evm:~# ls -l abc.yuv
-rw-r--r-- 1 root root 0 Dec 31 10:42 abc.yuv
Pleas help to resolve.
Thanks,
Sudheer.