Dear all:
Now I designed a board use DM8127 refer to the appro design,RDK vision is 3.5.0 . When “CCCC” characters appear on TeraTerm ,I load the u-boot.min.uart to the board,but after finished load ,it can,t appear prompt “TI-MIN#” ,it doesn,t work! the appro desigener used four 128M DDR3 altogether 512M,but I used two 128M DDR3 altogether 256M,and used the same DDR3. is it related to the matter? I must to modify anywhere? Meanwhile ,I made a SD card to boot the board ,it could work on the appro board ,but when I used on my board ,changed the boot mode to SD mode ,power on , nothing appear on the console ,it can,t work too, why? help me out! thank you very much!