Hi,
I have compiled the capture_encode application and trying to run on the evm but it fails with below errors:
root@dm814x-evm:/home# ./capture_encode_a8host_debug.xv5T -o sample.h264 -m 108
0p -f 60 -b 1000000 -d 0 -n 1000
output file: sample.h264
bit_rate: 1000000
frame_rate: 60
num_frames: 1000
mode: 1080p
display_id: 0
Capture-Encode example
===============================
[t=0x00000004] [tid=0x400a5000] xdc.runtime.Main: ERROR: "IpcSupport.c", line 148: ipc_initialize(), error in ProcMgr_open()
xdc.runtime.Main: "IpcSupport.c", line 148: ipc_initialize(), error in ProcMgr_open()
[t=0x000001e5] [tid=0x400a5000] xdc.runtime.Main: ERROR: "IpcSupport.c", line 231: ipc_initialize() failed
xdc.runtime.Main: "IpcSupport.c", line 231: ipc_initialize() failed
[t=0x0000035e] [tid=0x400a5000] xdc.runtime.Main: ERROR: "IpcSupport.c", line 148: ipc_initialize(), error in ProcMgr_open()
xdc.runtime.Main: "IpcSupport.c", line 148: ipc_initialize(), error in ProcMgr_open()
[t=0x0000043b] [tid=0x400a5000] xdc.runtime.Main: ERROR: "IpcSupport.c", line 231: ipc_initialize() failed
xdc.runtime.Main: "IpcSupport.c", line 231: ipc_initialize() failed
[t=0x00000514] [tid=0x400a5000] xdc.runtime.Main: ERROR: "IpcSupport.c", line 148: ipc_initialize(), error in ProcMgr_open()
xdc.runtime.Main: "IpcSupport.c", line 148: ipc_initialize(), error in ProcMgr_open()
[t=0x000005e6] [tid=0x400a5000] xdc.runtime.Main: ERROR: "IpcSupport.c", line 231: ipc_initialize() failed
xdc.runtime.Main: "IpcSupport.c", line 231: ipc_initialize() failed
capture_encode_a8host_debug.xv5T: DomxProcMgrIf_HLOS.c:287: DomxCore_mapPhyAddr2UsrVirtual: Assertion `(pSlaveProcHandle != ((void *)0))' failed.
Aborted
root@dm814x-evm:/home#
Any pointers on what I am missing ?
Thanks And Regards,
Mike