Hello,
We are using DM8148 with DVRRDK_03.50.00.05. We are using the following pipeline,
Capture(720p@50) --> DEI & Resize --> SwOSD(DSP) --> Display (720x576).
With this pipeline we are seeing a latency of around 190msec.
In my prints says,
DISPLAY: SDDAC(SEC1): 12 fps, Latency (Min / Max) = ( 255 / 0 ), Callback Interval (Min / Max) = ( 255 / 0 ) !!!
Latency Min and Callback Interval Min numbers seems to be not convincing.
We are expecting around 100msec.
I have gone through the following links which suggest to implement display ISR which helps to improve 1fps (40msec), but still not close to as expected.
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/282790
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/249459/904005#904005