Hello,
I use DM8148, and wanted to use jffs2, which requires to change the default ecc from BCH8 ->HAMMING HW.
I made modifications in both kernel and u-boot:
And also verified that I program everything with:
nandecc hw 0.
But the 1st stage u-boot does not start (there is no printing at all after reset)
I would like to ask if I there is some additional step I need to do.
How does the flash nand knows after reset that it needs to read from address 0, with hamming ecc ?
Thanks you,
Ran