hi all
I'm working on a project where I use the DM8127
The hardware I use is very similar to the appro IPNC DM8127 hardware.
One of the few things that are different is the memory, I use 2Gib instead of 512 Mb (the new memory is k4B4G16).
I've updated the file ddr_defs_ti814x.h:
#define PG2_1_DMM_LISA_MAP__0 0x0
#define PG2_1_DMM_LISA_MAP__1 0x0
#define PG2_1_DMM_LISA_MAP__2 0x0
#define PG2_1_DMM_LISA_MAP__3 0x807C0300
According to the board layout files A13 and A14 are connected between the DDR and the dm8127,
but I still seem to use only 512Mb of memory (I read the the same data from 0x80000000, 0xA0000000, 0xC0000000 and 0xE0000000)
I can see this problem both from the ARM (uboot) and from the DSP
I assume there is another configuration I need to change, but I can't find what it is.
Assuming the problem is software and not HW, What else can cause this problem?
Thanks,
Hagai