Hi,
I am using TI8148 EVM board, linux-2.6.37-psp04.04.00.01 and hdvpss_01_00_01_44 firmare.
I am using ti814x_hdvpss_1G.xem3 newly compiled and generated firmware. I could able to use this firmware using the v4l2 application i.e. saLoopBack.
I want to debug and use UIA loges but I am not getting the logs.
procedure used:
On the target we are running the saLoopBack application and on host using telnet, connecting to the EVM board and running the application
" /usr/share/ti/ti-uia/loggerSMDump.out 0x9ae00000 0x100000 all"
I have tried with different address i.e. 0x9E400000 and 0x8F000000 but could not get the UIA logs.
Is the newly compiled and generated v4l2 firmware ti814x_hdvpss_1G.xem3 has UIA enabled ?
If enabled what is the address argument we need to use for loggerSMDump.out application ?
If UIA is not enabled in the firmware ti814x_hdvpss_1G.xem3 how to enable it?
How can we enable the UIA by default in firmware itself and print the logs using the loggerSMDump applicaion?
Please help to enable the UIA debug logs.
Thanks,
Sudheer.