Hi,
The goal is to be able detect face features (to start with, eye) on the DSP available on DM8127 (C6748). I thought the best option available is to train the OpenCV Haar classifier for eye detection and store the generated xml file on the DM8127 flie system. Then instantiate the OpenCV cascaded classifier on the DSP and use it to detect faces in an input image. However, finding OpenCV which would run on C6748 has not been very easy. Finally I saw from the below link that OpenCV version 1.x was ported to C6748 and is in fact used in a face detect demo on C6748:
In the link they say that the code for the face detect demo is available along with the necessary opencv libraries in the BIOSC6SDK and the link to download it from is:
software-dl.ti.com/.../index_FDS.html
However, whenever I click on the link for bios_c6sdk_02_00_00_00_setupwin32.exe, it just gives me the below error:
An error occurred while processing your request.
Reference #97.2c32d417.1435686232.26955d76
So my questions are two fold:
1) Is there another link from where I could download the BIOSC6/SDK?
2) Is there another place where some version of OpenCV libraries compatible with C6748 be downloaded?
Thanks everyone for your time.
Regards,
Sreenath K R