Hello,
I have some strange issue.
when using /dev/fb0 - everthing works perfect.
But on using /dev/fb2 I have issues.
with psplash it works OK (I need to compile with source code using /dev/fbv2) , and I see the output in sd output.
But with qt application it always get to digital output.
I then tried to always force it use /dev/fb2 as following:
ln -s /dev/fb2 /dev/fb0
check with psplash - it works ok (and the output goes to sd, when compiled in source as "/dev/fb0")
check with qt - still using the wrong output (digital).
In all cases I use:
new:
insmod ./kermod/ti81xxfb.ko vram=0:1M,2:48M
(instead of
insmod ./kermod/ti81xxfb.ko vram=0:48M,2:1M
)
It is quite a strange behaviour.
Any idea what's wrong ?
Regards,
Ran