Hi TI experts,
I'm in customized DM385 platform IPNC_RDK 3.5
In this Using crop function Vdis_SetCropParam() able to crop 480*640 in swMs link
In display side enabled the i/o resolution to 480*640
After this, Camera start in progress to (848 * 480), applying mirror command it has to rotate to (480 * 840) while entering to swMs (expecting 480 * 640) but still I'm getting (480 * 848)
Whare & What it could be the issue ???
Kindly suggest me to solve this issue !!
Regards,
Rajesh Kannan.S