Hi All
I am using aptina AR0331 sensor for DM8127 for camera
I am getting HSYNC and VSYNC on the proccessor side and try to capture data via parallel interface of ISS CAM Port to SDRAM
The ISS supports three simultaneous pixel flows (Stallcontroller, CSI2 A, and parallel interface [CPI]), but only one of them at a time can use the image processing hardware(ISP); the others can go directly to memory
I am configuring CBUFF interface of ISS to capture data. However i am not getting any captured data in SDRAM
Below are my configuration for CBUFF.
>Virtual address space upper threshold:0x84000000
>Virtual address space upper threshold:0x8FFFFFFF
>Physical address:0x80000000
>Window size upper threshold:1080
>Window size upper threshold:0x0000
Can anyone help me in this regard?
Thanks
Akhil