Hi,
Working on DM8148 , ti-ezsdk / omx_05_02_00_46 .
I use the application decode_display.
My project is to decode h264 file and disply it on CVBS channel. For this I omitted the Scalar component,
so that the disply component will receive yuv420.
The problem was that the DEC component receive the h264 frame (activate IL_ClientCbEmptyBufferDone call back function) but did not continue with the process (did not activate IL_ClientCbFillBufferDone) and nothing was displayed . No error was reported.
Best Regards,
S.W