Tool/software: Linux
Hello,
I would like to verify if bch8 is supported with dm8148.
Best Regards,
Ran
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hello,
I would like to verify if bch8 is supported with dm8148.
Best Regards,
Ran
Ran Shalit said:When using jffs2 we've encountered ecc errors with HW ecc , so we moved to SW ecc.
As I understand jffs should be able to work with both of them, Right ?
Yes. Due to constrain of metadata layout in OOB area, only '1-bit Hamming H/W' or '1-bit Hamming S/W' ECC schemes can be used with JFFS2 File-system
Ran Shalit said:So with the latest PSP version I can use:
ubifs with 8-bch, using it from both u-boot & linux (read/write from one and write/read from another ),
Right ?
Yes. You should also revert back the BCH16 related linux kernel patches, for proper BCH8 operation in linux kernel.
See also:
Regards,
Pavel