Tool/software: Linux
Hello,
We try to record both graphic and video. Our main output (which contain both graphic and video from pipeline) is DVO2 (which is tied to HDMI+SD)
But - CaptureWB does not work (and it never worked + no support for that in e2e), so our only hope is to use SD output and connect it back as input into VIP port B, so that we can now record graphic+video.
But using the SD, bnow we have another problem:
SD does not show the same graphics as HDMI !
I would please like to understand what is the relation between /dev/fbX and physical output (hdmi, SD).
Do we need to configure fbX to get to SD/HDMI.
With our previous tests we saw that fbX can be displayed in HDMI but not in SD, even when they are tied !
This is very important issue for us and the only hope to make it work,
Thank you for the help,
Regards,
Ran