Tool/software: Linux
Hello,
We recently noticed that there are different clock rate observed in linux compared to u-boot.
In u-boot we see:
U-Boot 2010.06-dirty (Dec 26 2016 - 10:37:28)
TI8148-GP rev 3.0
L3 clk : 200MHz
IVA clk : 410MHz
ISS clk : 480MHz
DSP clk : 750MHz
DSS clk : 200MHz
ARM clk : 720MHz
DDR clk : 400MHz
While in linux with cpuinfo or sysfs entries we see 1GHz rate.
The chip revision should be limited to 720Mhz.
1. How is it that the clock rates is different ?
2. We tried to change rate to 600MHZ with sysfs scaling_setspeed , but it fails to change to 600M (although it appears in sysfs entry for available frequencies)
Thank you,
Ran