Hi
I have compile ti8148 dvr_rdk package and running default use cases (4CH VCAP + VENC + VDEC + VDIS - Progressive SD Encode + Decode).
Am saving the captured, encoded frames to a file.
While the usecase is excecuting, enabled Motion detection using the run time menu.
Capture Settings -> SCD mode selection -> Enable Motion detection on Channel-0
Added log in the function (Demo_eventHandler) to know the event been received by the demo app.
I can only see the initial event recevied for HDMI/TV connect as below:
DEMO: Received event == [0x0006]
But no log for Motion detect event receive is captured, once i enabled Motion detection as above.
To check Motion event below is what i have done,
Start the demo app -> enable save -> point to camera to a idle spot -> enable Motion detect using runtime menu.
Need Info on below items:
1. How to test Motion detection on TI8148 dvr rdk using demo app.
2. is there any specific change need to made to the default app for motion detection.
Thanks in advance