Hello,
I am developing a device containing AM3874. The board is custom. The prototype was fitted with DDR3 400 MHz which works ok, but I would like to use faster RAM (at least 675 MHz). Theoretically the processor can work with up to DDR3-1066 but I found that there is no such option in u-boot configuration, only 400 and 533 MHz options available (I've checked arch/arm/include/asm/arch-ti814x/ddr_defs.h). What has to be done in order to work with DDR3 675 MHz or even 796 MHz? Is it possible?