Hello,
I am trying to build nsp_gmacsw_4_15_00_00.
using below versions of libs:
set NDK_ROOT=c:/ti/ndk_2_24_02_31
set BIOS_ROOT=c:/ti/bios_6_46_04_53
set TIARMCGT_ROOT=C:/ti/compiler/arm_5.2.4
set GCC_ROOT=C:/ti/compiler/gcc-arm-none-eabi-4_7-2013q3
set CGT6X_ROOT=C:/ti/compiler/c6000_7.4.2
set XDC_ROOT=c:/ti/xdctools_3_32_01_22_core
using "xdc all" for building and i see below error:
"making package.mak (because of package.bld) ...
js: "./config.bld", line 85: xdc.services.global.XDCException: xdc.PACKAGE_NOT_FOUND: can't locate the package 'ti.targets.elf' along the path: 'c:
/ti/xdctools_3_32_01_22_core/packages;../../..;'. Ensure that the package path is set correctly.
xdctools_3_32_01_22_core\gmake.exe: *** No rule to make target `package.mak', needed by `.interfaces'. Stop.
Done."
Any suggestion, what could be the issue?
Regards,
Tejeswini