1)Dose ezsdk_5_02_01_59 allow the user to control i2c bus from linux?
2)is there any way to change the config of tvp7002 to support vga input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1)Dose ezsdk_5_02_01_59 allow the user to control i2c bus from linux?
2)is there any way to change the config of tvp7002 to support vga input?
Hi,
My answers.
1. Currently TVP7002 is controlled through media controller binary. So it is not possible to change the TVP7002 driver to support VGA input.
2. Its not possible since media controller source is not available as a part of ezsdk.
We have plan of moving the TVP7002 control to Linux TVP7002 driver. But in that also VGA resolution is not supported.
Regards,
Hardik Shah
thanks you very much!
but when the plan of moving the TVP7002 control to Linux TVP7002 driver will finish?
can your give me a accurate time?
Hi,
Plan for supporting TVP7002 Linux driver is 4Q11.
Regards,
Hardik Shah