Hi
I try to use the following c function to mount a nfs directory in my c program on a DM8168 DaVinci EVM board using EZSDK 5.02.
mount("10.112.12.150:/home/chan/media", "/home/tt/media", "nfs", 0, "-o nolock");
It always fails. However, the C function, umount(), is working.
Even when I do the mount in the console, "mount -o nolock 10.112.12.150:/home/chan/media /home/tt/media" would fail, but put busybox before this mount command would make it work.
busybox mount -o nolock 10.112.12.150:/home/chan/media /home/tt/media
Any kind of help is appreciated.
Wai Kwok