Hi, we use DM8168, TVP5158, RDK4.0.
The data flow is:
There has a strange problem.
The setting of DEI_0 and DEI_1 is same just the ID is not, one is SYSTEM_LINK_ID_DEI_HQ_0 and the other is SYSTEM_LINK_ID_DEI_HQ_1.
I set the channel number for DEI_0 is 0, 1, 2, 3, and the another dup output is 4,5,6,7, just channel 0 duplicate to channel4.
I static the procced frames in VcapVenc_bitsWriteMain() for every 30s.
If the input for channel 0 is PAL, the encoded frames are only 625, but the channel 4 is 750.
If the input for channel 0 is NTSL, the encoded frames are 750, but the channel 4 is 900.
What's the problem?