Hi,
I have a custom H.264 SVC Encoder running on M3-HDVICP in DM388/DM8127, and would like to integrate this into IPNC RDK's McFW. I know the current Enc Link supports H.264AVC, So I need to create my custom link for my Encoder.
My Question is :
1. Is it supported on IPNC RDK to write custom links? I have already purchased IPNC RDK 3.8 ver.
2. If not,what are the special components (Like M3 Source codes?) I need to get before starting to create a custom link?
Pls reply.
Best Regards
JK