Hello,
We are trying ro run an application on DSP. For that we have to get data from Vpss to DSP and then bacl to VPss. We have a VpssFramesOut->DspFramesIn->ALG->DspFramesOut->VpssFramesIn link setup. This is not working. So we removed ALG and connected the rest. Still not working. We then removed the DSP part and still it is not working. Now we have only VpssFrameOut->VpssFramesIn and it is not working and the error message is:
On M3VPSS side:
[m3vpss ] 62295: NOTIFY: Send Event to [VPSS-M3][22] failed !!! (status = -14)
[m3vpss ] 62295: Assertion @ Line: 69 in links_common/system/system_ipc_notify.c: status == Notify_S_SUCCESS : failed !!!
What could be the possible reason this error is coming?
Thanks