Hi,everyone, I enconter a strange problems about uboot in the DM8168 DVRRDK 4.1.
I find different cross_compile woud get different u-boot.bin.noxip file and one can boot up from nand flash while the other can't after I modified the DDR freq from 796.5 Mhz to 675 Mhz depend on our boards.
I use the arm-none-linux-gnueabi and arm-arago-linux-gnueabi- to compile the uboot.
1、CROSS_COMPILE= arm-none-linux-gnueabi-:
The output file uboot.bin.noxip can boot from the Nand flash .
2、CROSS_COMPILE= arm-arago-linux-gnueabi-:
The output file uboot.bin.noxip boot from the nand flash but there is nothing to be printed.When I use CCS debug it ,I find it has configured the DDR and copied itself to OCRAM and DDR .Even though it looks like to run ok ,it prints nothing, Why ?
Besides,I set the PC register to 0x40400000 and click the RUN by CCS, it runs OK again and prints some informations likes cpu freq .
what is the reasons of these ? Can someone explain or give some suggests ? Thank you very much.
Looking forword to your reply .