Hi,
We got following log when we use SwMsLink_drvDoDma function in swMsLink_drv.c. we use rdk4.1 as code base to develop our usecase. the system still work normally after this log appear. Any problem cause this log appear? it will cause any problem in my system? Thanks.
irq 14: nobody cared (try booting with the "irqpoll" option)
Backtrace:
[<c0045bdc>] (dump_backtrace+0x0/0x110) from [<c03a6828>] (dump_stack+0x18/0x1c)
r7:00000000 r6:00000000 r5:c054fec4 r4:c054fec4
[<c03a6810>] (dump_stack+0x0/0x1c) from [<c0097090>] (__report_bad_irq+0x38/0x90)
[<c0097058>] (__report_bad_irq+0x0/0x90) from [<c009723c>] (note_interrupt+0x154/0x1d8)
r5:c054fec4 r4:c054fec4
[<c00970e8>] (note_interrupt+0x0/0x1d8) from [<c0097f54>] (handle_level_irq+0xcc/0x11c)
r9:0000000a r8:d8000000 r7:00000002 r6:00000000 r5:0000000e
r4:c054fec4
[<c0097e88>] (handle_level_irq+0x0/0x11c) from [<c003707c>] (asm_do_IRQ+0x7c/0xa0)
r5:c0535f40 r4:0000000e
[<c0037000>] (asm_do_IRQ+0x0/0xa0) from [<c03a88f4>] (__irq_svc+0x34/0xa0)
Exception stack(0xc0535e98 to 0xc0535ee0)
5e80: 00000008 c053a5b0
5ea0: 00000000 c05a4800 c0534000 00000000 00000000 00000002 d8000000 0000000a
5ec0: 0000001f c0535f14 c0535f18 c0535ee0 c006ddc4 c006dcbc 20000113 ffffffff
r5:fa200000 r4:ffffffff
[<c006dc74>] (__do_softirq+0x0/0x108) from [<c006ddc4>] (irq_exit+0x48/0x94)
[<c006dd7c>] (irq_exit+0x0/0x94) from [<c0037080>] (asm_do_IRQ+0x80/0xa0)
[<c0037000>] (asm_do_IRQ+0x0/0xa0) from [<c03a88f4>] (__irq_svc+0x34/0xa0)
Exception stack(0xc0535f40 to 0xc0535f88)
5f40: 81600281 40000013 c0535f88 00000814 00000816 c0583780 c002c0a0 c0538084
5f60: d8000000 413fc082 0000001f c0535f9c c0535f88 c0535f88 c0042fac c0042fb0
5f80: 20000013 ffffffff
r5:fa200000 r4:ffffffff
[<c0042f44>] (default_idle+0x0/0x78) from [<c0043558>] (cpu_idle+0x50/0x90)
r5:c0583780 r4:c0534000
[<c0043508>] (cpu_idle+0x0/0x90) from [<c03a0374>] (rest_init+0x60/0x78)
r5:c0583780 r4:c05a79ec
[<c03a0314>] (rest_init+0x0/0x78) from [<c0008cc8>] (start_kernel+0x274/0x2cc)
[<c0008a54>] (start_kernel+0x0/0x2cc) from [<d8008048>] (0xd8008048)
r6:c002c09c r5:c058389c r4:10c53c7d
handlers:
[<c004b714>] (dma_ccerr_handler+0x0/0x1fc)
Disabling IRQ #14