I tried to run the code that Cory Tusar wrote at
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/189059/712138.aspx
I added the code to the u-boot of the Z3-DM8168-PCI-RPS board, calling pcie_init() from s_init(). The board is set to NAND boot mode. I need to run the board as PCIe Endpoint and load the software from the NAND. The board is inserted to a PCIe slot of a PC host.
Booting the host PC with Windows 7 or with Ubuntu 14.04, both did not show the card in the PCI device list.
Can anyone help?
Does anyone have the DM8168 ROM code of initializing the PCIe as Endpoint for the PCIE boot mode?