Hello.
We have our own device on base of DM8168 with DDR2. We have made all necessary changes to move to the ddr2 memory. We have collected own images of the MLO, u-boot.bin, uImage and file system, and used special ti script to write all these on SD card. Our debug port is uart2. After powering up there was no any of messages in the console. We connected through the debugger and verified that MLO uploaded at 0x40400000 address correctly. Moreover, we have written down the own code in the MLO sources and were convinced that he has completed its work correctly. After connecting the debugger, value of PC counter register is 0x20080. Please suggest what could be the problem and what we need to do to solve it.
Thanks,
Dmitry