In one of our Custom DM8168 board,while connecting JTAG through Code compressor studio executing "GEL file"
We are observed the following issue
-----------------------------------------------------------------------------------------------------------------------------------------------------------
CortexA8: GEL Output: EVM816x Startup Sequence
CortexA8: GEL Output: PRCM Setup Complete
CortexA8: Output: Main PLL Init is in Progress, Please wait .....
CortexA8: Trouble Writing Memory Block at 0x48140400 on Page 0 of Length 0x4: (Error -2130 @ 0x48140400) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0) CortexA8: GEL: Error while executing OnTargetConnect(): Target failed to write 0x48140400 at *((unsigned int *) (0x48140000+0x400))=(unsigned int) main_pll_ctrl [CABS_AVRM_sd_SW_level_allCS.gel:325] at mainPLL(64, 0x1, 0x8, 0x800000, 0x2, 0xE, 0x0, 0x1, 0x8, 0xAAAAB0, 0x3, 0x9, 0x55554F, 0x3, 0x9, 0x374BC6, 0xC, 0x48, 0x4) [CABS_AVRM_sd_SW_level_allCS.gel:877] at Setup_MainPLL() [CABS_AVRM_sd_SW_level_allCS.gel:46] at OnTargetConnect() . CortexA8: Trouble Reading Register CP15_Registers_CP15_CONTROL_REGISTER: (Error -2131 @ 0x20013F00) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0) CortexA8: Failed CPU Reset (HW): (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0) CortexA8: Trouble Halting Target CPU: (Error -1260 @ 0x0) Requested operation failed for security violation. Check security/priviledge settings, and retry the operation. (Emulation package 5.1.507.0) CortexA8: Trouble Halting Target CPU: (Error -1260 @ 0x0) Requested operation failed for security violation. Check security/priviledge settings, and retry the operation. (Emulation package 5.1.507.0) CortexA8: Trouble Halting Target CPU: (Error -1260 @ 0x0) Requested operation failed for security violation. Check security/priviledge settings, and retry the operation. (Emulation package 5.1.507.0).
----------------------------------------------------------------------------------------------------------------------------------------------------------
We have checked power sequence & system clk seems to be ok. we even tried with reducing JTAG TCLK also, the same GEL file executing properly in remaining boards. Kindly let me know your suggestions/Inputs
Thanks & Regards,
Vijay Varma