Hi All,
I use the RDK4 on DM8168 platform, and TVP5151 as SD video decoder, it's output is single channel interlaced video data. Now I can get top filed data and bottom filed data separately when using captureLink, but I need one whole frame that contains top and bottom filed, so I have the two questions as follows:
1. Whether can I get one meragedFileded frame when the video decoder(such as TVP5151) is interlaced output? If yes, how to do it( DVRRDK4 and DM8168)?
2. If I can't, how the DEILink deals with the top/bottom field data when the chain is captureLink->nsfLink->deiLink? we know that the DEI deals with the fieldMeraged frame and deinterlace, but the top/bottom field data is in separated buffer now.
Thanks and Regards,
Jason Lee