Hi there,
we have problem on our custom dm8168 board, this is happend on our reversion 3 board, we are using EZSDK 5_05_02_00 with latest DVRRDK hdmi hdcp patched, for the previous version, HDCP on the HDMI is alway fine, but it is failed on the latest version, we checked our hardware design, there are no big changes with the 2nd version, all the design relate the on-board hdmi remain the same, then we checked the ddc i2c bus of HDMI with oscilloscope, and also print kernel debug information of hdcp, it seems, that the dm8168 and receiver(HDCP compatible monitor ), can send AKSV, BKSV and random number AN correctly, the only problem is the R value in dm8168's register is not equal to the R' which read from receiver, which cause he HDCP handshake failure, we also check the part number of the dm8168, it seems nothing special, it using the same cpu with the last version, is anyone have any idea, thank you in advance.
Kevin