hi,
is it possible to accessing PowerVR from inside DSP?
best regards
Max
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
is it possible to accessing PowerVR from inside DSP?
best regards
Max
Max,
The PowerVR core is part of the SGX Subsystem, thus we will have a look if SGX SS can be accessed by the C674x DSP.
Based on the DM816x datasheet, the answer is no, C674x DSP can not access SGX SS. See Table 6-1. L3 Master-and-Slave Connectivity - from this table we can see that only Cortex-A8 ARM (M2 64-bit port) can access SGX at address 0x56000000.
Best regards,
Pavel