Hi
I am using the latest EZSDK, 5_05_02_00 for DM8168 board. If I want to use TVP5150 as a capture device, what changes needs to be done in the source code. By default the TVP7002 chip is used for capture. I have seen the Limitations in the release notes (ezsdk_5_05_02_00_dm816x_Release_Notes.pdf) as like below:
External video capture is only supported through the TVP7002 video decoder via I2C1. Customers are required to maintain the same configuration on their boards. The EZSDK will support additional capture devices in future releases. Customers will also be able to add capture devices of their choice in future releases.
Whether this SDK supports other TVP chip apart from TVP7002. If not, when the next release will be done from TI.
Thanks in advance.
Regards,
Salih