Hello.
We have been working with ksz9021gn PHY connected to DM8168. But work is possible only at 10Mbps on our custom board. The link at 100Mbits and 1000Mbits are presented, but ping command is not passed. We refer to the manufacturer of the controller-he said that we have a correct scheme. We checked the frequency-all right. We have removed twice all of the components that are relevant to the PHY and PHY too. But the result did not change and we still have the 10Mbps speed only. Please help to understand what the problem is. Are we need to do something in driver? We are using last SDK without applying patches. We have some expirience working with other PHY - they had not had any problems. Problems began only when we decided to put a new ksz9021gn PHY.
Dmitry.