Hi,
Our DDR's frequency is configured in uboot as below
#define CONFIG_TI816X_EVM_DDR3
#define CONFIG_TI816X_DDR3_796
1) Maximum ddr clock rate is 796MHz in ti8168 platform?
2) The maximum frequency of our DDR is 1333MHz, why the uboot 796MHz setting is ok? it should be DDR 1600MHz?
Sorry I am new about DDR and any help will be appreciate.
Thanks
BR,
Steven